Other Parts Discussed in Thread: BQ24070, BQ24072
Hi,
My customer is having issues with their bq24030 design because their system occasionally requires drawing battery currents higher than the 4A abs max. They are looking into disconnecting OUT (leave floating), and tying the system load directly to the battery. Do you see any issues with this configuration (pretty much using as a non-powerpath charger)? These are the drawbacks I already communicated to them:
• If the battery is deeply discharged, the system will not power on until the battery is charged beyond the system UVLO.
• The battery charge rate will be the programmed charge current minus the current being drawn by the system, so charge time might increase depending on the system.
• You have lower power from the charger since the system will not see the 5V/4.4V. The charge LDO will drop it down to the battery voltage.
Thanks,
Antonio