Part Number: REF5030
If I have 3.3V input, and 3.0V output, what are the loading and temperature conditions for that to remain true?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: REF5030
If I have 3.3V input, and 3.0V output, what are the loading and temperature conditions for that to remain true?
Hi Lauren,
The worse case condition is 125C. At 125C the REF5030 with 3.3 VIN can only output 3mA output based on the typical graph of figure 6.
You can use figure 6 to get a good idea of the worst case conditions.
Most ADCs do not consume more than 1mA.