Part Number: LM3431
Provide complete circuit diagram: Provide complete circuit diagram
Problem 1: There is a strange sound when the light is on.
The picture shows the measurement waveform of Q 5-D terminal
Adjusted 1.R39, R37 frequency part without improvement
2.R31, R26 total watts part no improvementTURN-SCH.pdf
3.R71, R73, R75 have not improved
Please help to see if there is any adjustment needed