Part Number: LM34922
i am using LM34922. Can you give me bill of material and schematic for 12v input, 12V output and 2A current limit?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM34922
i am using LM34922. Can you give me bill of material and schematic for 12v input, 12V output and 2A current limit?
Hi Dipanshu,
I currently do not have this information, but will look into this.
Regards,
jenson
Dipnbshu,
LM34922 has a minimum off time so for 12 V input, the output voltage is less than 12 V. If you have 12 V, why not power your load directly from it?