Other Parts Discussed in Thread: UCD3138064
Tool/software: Code Composer Studio
Hi everyone, i need to generate dpwm waveform ,for this i have referred videos in ti website, but couldn't able to get dpwm waveform. Could you please tell me is there any necessary hardware connection get dpwm waveforms. I have atttached the code, is there any changes to make in code?
[code]
#define MAIN 1 #include "system_defines.h" #include "Cyclone_Device.h" #include "pmbus_commands.h" #include "pmbus_common.h" #include "pmbus_topology.h" #include "variables.h" #include "function_definitions.h" #include "software_interrupts.h" #include "cyclone_defines.h" #include "stdio.h" #define PCLK_PERIOD         4.0e-9 #define PERIOD_SECONDS      10.0e-6 #define PERIOD_CLK          ((int)(PERIOD_SECONDS/PCLK_PERIOD)<<4) #define EVENT1              (int)(PERIOD_CLK*0.00) int ram_event2; void inti_dpwm(void) {     Dpwm0Regs.DPWMCTRL0.bit.PWM_MODE = 0;  // Set to normal mode     Dpwm0Regs.DPWMCTRL0.bit.CLA_EN = 0;     Dpwm0Regs.DPWMPRD.all = PERIOD;     Dpwm0Regs.DPWMEV1.all = EVENT1;     Dpwm0Regs.DPWMCTRL0.bit.PWM_EN = 1;     LoopMuxRegs.GLBEN.bit.DPWM0_EN = 1; } void main() {        if(GioRegs.FAULTIN.bit.FLT3_IN == 0)// Re-Check pin assignment (ADC_EXT/SYNC may be?)     {         //clear_integrity_word();     } #if (UCD3138|UCD3138064)     MiscAnalogRegs.CLKTRIM.bit.HFO_LN_FILTER_EN = 0;     MiscAnalogRegs.CSTRIM.bit.RESISTOR_TRIM =23; //28; #endif //(UCD3138|UCD3138064)     init_pmbus(0x58);     init_dpwm();     ram_event2 = Dpwm0Regs.DPWMEV2.all;     for(;;)         {             pmbus_handler();             Dpwm0Regs.DPWMEV2.all = ram_event2;         }     }[/code]
Thanking you.