This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MC33063A: MC33063A application schematic

Part Number: MC33063A

picture1 is from datasheet ,picture2 is Schematic for 24V input and 5V output,max current is about 900mA

picture1 and picture2 all use pnp transistor,but some places is different(please see green circle).

for exemple:

1. pin1,pin8 and pin2 

2. No series resistor on the outside of the pin1 in picture2

3. please help to check if schematic in picture2 is correct or not?


Thanks