Part Number: BQ79606A-EXAMPLE-CODE
Hi Team,
May I learn from you when we should call this API - CommClear()?
Need more example on this function.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: BQ79606A-EXAMPLE-CODE
Hi Team,
May I learn from you when we should call this API - CommClear()?
Need more example on this function.
Hi,
A Communication Clear is used to clear the UART receiver and instruct it to look for a new start of frame. An example when this is useful is if the device is waiting for a response from the stack devices but it didn't receive all the bytes expected. You can send a comm clear (by holding the RX line low for a min of tUART(BRK) bit periods) and this way the receiver will detect the next instruction received as a start of a new frame.
Please review section 8.5.1.1.1.4 "Communication Clear (Break) Detection" in the device datasheet for more details.
Best regards,
Leslie
Hi,
Thanks for your comments. Yes, I can find "Comm clear" description on TRM. However, I am looking forward more information. BTW, may I have a example code when you will call this function during SW implement?
Hi
Comm clear is taking RX pin low for tUART(BRK)
I don't know how we can provide example code for this.
Thanks
Roger