This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25942A: TPS25942A design

Part Number: TPS25942A
Other Parts Discussed in Thread: TPS2663, TPS2660

hi

i want to use the TPS25942A to monitor a VIN to the system of 18v(nominal)
is there a way to set the Over voltage to monitor ~19v? 
i dont see it in the tool, and not sure it possible - but in TI website - it says up to 20
what should be the resistors for such a design?
thanks

  • Hi Tzachi,

    Thanks for reaching out.

    We recommend to use OVP under 18V which is the max recommended operating voltage of the device. For higher voltage support, please look at TPS2660, TPS2663 devices.

    Best Regards, Rakesh