Other Parts Discussed in Thread: MC34063A, , LM5119, PMP10979, LM25119
Hello, I need to design a buck converter that will limit the voltage in an automotive-type dc system. The input may be from 11 to 15 volts; the output should be regulated to a maximum set point (e.g. 13 volts). So if the input is higher, the output stays at that set point; if the input is lower, it would simply follow the input voltage (as closely as possible). Output should be about 60 amps. But it needs to be very inexpensive. I was hoping to utilize either an MC34063A, a UC3525A, or something similar, maybe with gate drive circuits added, and maybe two of them for two-phase operation (if they can be synced that way and if it’s cost effective). But I have found very few application notes related to this type of thing. I’m looking for a control IC that’s under a dollar, if that's possible. Can you suggest anything for this application? Thanks!