This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMG5200: Question about Feedback control (Analog vs microcontroller)

Part Number: LMG5200
Other Parts Discussed in Thread: TIDA-01168, LM5170,

Hello, 

Our group is currently using the LM5170 current controller to control our current similar to the power stage for the TIDA-01168 schematic.

We want to start integrating the LMG5200 GaNFET to see and compare the differences between Silicon MOSFETs and the GanFETs.

We're trying to do research on how to integrate the LMG5200 into our design, but we are fairly new to this.  

Our question is whether we can directly control the LMG5200 using the LM5170 or using a separate microcontroller.  We're not sure whether there is a step we have to do specifically for the GaNFET or not.

We want to figure our how to integrate the LMG5200 into our current schematic that we have.  We believe we have the LM5170 working as a bidirectional DC-DC converter.  Our goal is to eventually compare the results and efficiency of our current design with one that contains a GaNFET.

Any help or steps on what to do to integrate the GaNFET would be appreciated!

Attached below are the datasheet links of the files we are using.

http://www.ti.com/lit/ds/symlink/lmg5200.pdf - LMG5200 datasheet

http://www.ti.com/lit/ds/symlink/lm5170-q1.pdf - LM5170 current controller that is currently used

http://www.ti.com/lit/ug/tiducs2b/tiducs2b.pdf - TIDA-01168 power stage reference design being used; figure 18 

Our current schematic is also linked below.  It contains the power stage mentioned in the TIDA-01168 design.

bidirectionalDCDCbuck_2-25-2020.TSC

  • Hello,

    Thanks for your interest in GaN. LMG5200 is not very different than any other Si power stage which includes driver and FETs. There is no specific step that you need to do with LMG5200. However, due to the fast switching of GaN, you do need to pay attention to your layout to minimize the parasitic inductance. LMG5200 datasheet would be a good source for you to take a look regarding layout. Other than that, I think you would be fine. 

    Thanks and regards,

    Lixing

    Systems/Applications engineer

    Texas Instruments