This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61088: About maximum current limit

Part Number: TPS61088

Hi,

My Customer want to know the limit of the current value that can be set by Rlim.
(Customer want to increase the output power as much as possible.)
It is separately thinking about the problem of heat generation.
Please give your advice on Rlim limit and maximum output current setting.

Best Regards,
Yusuke

  • Dear Yusuke-San,

    The maximum current limit of TPS61088 is to set the Rlim=100k, if the Rlim value is lower than 100k, then the IC may can't handle such big power and results in thermal issue.

    What is the Vin range, Vo range and the maximum load current at the customer side?