This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMZM33606: Can SYNC clock be applied to SYNC/MODE pin of LMZM33606 before the LMZM is powered up?

Part Number: LMZM33606

 One of my customers is considering using LMZM33606 for their new products.

 They wants to send SYNC clock(5V-0V swing) to SYNC/MODE pin of LMZM33606 before the LMZM is powered up because the SYNC clock generator is powered up earier than the LMZM.

 I can see that the maximum voltage of SYNC/MODE pin is 5.5V in the device datasheet. So I think any diode is not inserted from SYNC/MODE to VCC.

 Is my understanding correct and is it no problem to apply 5V-0V clock to SYNC/MODE pin of LMZM33606 before the LMZM is powered up?

 Your reply would be much appreciated.

 Best regards,

 Kazuya.