Other Parts Discussed in Thread: BQ76940
Hello,
I am using the BQ76940 as a voltage/temp monitor for a 9-12 cell configuration with a different host MCU that will also drive external FETs for balancing. I understand that we need to bypass the existing balancing FETs on the EVM. My questions are the following:
1) What happens if the external balancing FET shorts a cell from the series (while keeping block voltages above Vshut), and in the worst case scenario, what would happen if one block falls below Vshut during balancing, but say i use R74 instead of R75 so that REGSRC gets its voltage from VCx10 instead of VCx5 (since the cells are just 2.3V)?
Thank you in advance.