Hi,
I'm working on a high current circuit which uses two drivers(UCC27712) to control a full-bridge IGBT module(MIEB101H1200EH). The drivers are powered by a 12V source and the full-bridge is powered by a 48V 62 amp source with a resistance load of 1 ohm . At a PWM frequency of 490 Hz the circuit works but there is a transient component in the transition between pulses that concerns me. Below I included a picture of the schematic and pictures of the signal(high-side of load referenced to ground) as I stepped the duty cycle through 20%, 40%, 60%, and 80%. If you have any insight into causes of this issue I would appreciate your input.
Thank you
20% Duty Cycle
40% Duty Cycle
60% Duty Cycle
80% Duty Cycle