Dear support team,
There is a figure 32 at the datasheet of TPS60401. It shows that shutdown control can be made with a push-pull inverting buffer. I have some quite small load: 200uA typical with 4mA as max load which needs a negative supply of something around -3V. I don't need any regulation but I want to be able to dim output voltage from -Vin down to 0 volts. Is it possible just to apply a PWM (500Hz is enough) to IN pin of these charge pump and get some PWM at its output?