This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A02: SOT-23 Package for TPS7A02 (3.3 and 1.8V)

Part Number: TPS7A02
Other Parts Discussed in Thread: TPS63020

Hi,

I'm looking for Ultra low Iq LDO for my battery powered application.

Battery --> Buck Boost(3.8V,TPS63020,)

Input 3.8V(constant) outputs are 3.3V @ 50mA max( to the uC which will be in sleep mode most of the time with current of 30uA).

Input 3.8V Output- 1.8V@ 10mA.

I'm looking for a SOT-23 package But i couldn't find on the Digikey, Only XDFN is available.

Thanks.

  • Hi Lakshminarayana,

    SOT-23 will be fully released by the end of the month. We actually have pre-production samples still available that you may use in the meantime. Full orderables part numbers are PTPS7A0218PDBVR and PTPS7A0233PDBVR.

    regards,

    Wilson