Hi Team,
We need a 3 battery input and 1 DC input power MUX for our Dual Camera Project.
The different power sources are:
1. Internal Battery-1(Vmax=16.8V, Vcutoff= 13V, Imax= 5.1A)
2. Internal Battery-2 (Vmax=16.8V, Vcutoff= 13V, Imax= 5.1A)
3. External Battery (Vmax=16.8V, Vcutoff= 13V, Imax= 5.1A)
4. DC Adapter (Vmax=15.5, Vcutoff= 13V, Imax= 5.1A)
We need a power mux to select between these sources.
Use Cases include.
a. Priority Battery Selection between Internal Battery-1 and Internal battery-2.(Priority to Internal Battery-1)
b. Once Internal Battery-1 reaches below set threshold voltage(13V for us), system should switch over to Internal Battery-2(if its voltage is >13V).
c. When both batteries are above the set threshold voltage, we should be able to select the one to power our system using control input from external processor.
d. Status outputs from the Power MUX regarding which power source is currently powering the system.
e. Once External battery is connected and its voltage is above threshold, system should switch over from internal battery to it.
f. If DC power is connected, system should be powered from it irrespective of other battery status.