Hi team,
I have several questions below about UCC28742:
(1) Vs pin can compensate the current-sense threshold across the AC-input range. What's the meaning?
(2) The gate drive turn-off current is internally limited to about 400 mA when DRV is above about 4 V. At lower DRV voltages the current will reduce, eventually being limited by the low-side on resistance, RDS(on). Why driving current is affected by Rdson?
(3) If additional blanking time is needed, a small bypass capacitor, up to 30 pF, can be placed on between CS pin and GND pin. How to explain bypass capacitor can influence blanking time?
Thanks.