I'm using BQ76PL455A-Q1 for measuring cell voltages and cell balancing.
However, certain cells of our battery (cell level / Lithium-ion, 18650, 4.2V, 2.5Ah, assembly level / 16 series and 4 parallels) was broken at almost 0V.
I still don't know whether or not there is a cause in the IC. so let me know.
Commands we transmit to the IC are as below.
Are there any factors that cause the broken cell to be unbalanced in the following commands ?
F2 10 10 E0 3F 35 |
F1 0E 10 54 5F |
F1 0C 08 55 35 |
F1 0A 00 57 53 |
81 00 0A 00 2E 9C |
92 00 10 10 20 B4 00 |
92 00 10 10 C0 B5 88 |
92 00 52 FF C0 59 AC |
91 00 3D 00 3C 6C |
91 00 3E BC 3D 2D |
91 00 07 00 2E CC |
91 00 0D 10 29 A0 |
94 00 03 FF FF 01 00 90 7D |
92 00 90 FF FF B9 BC |
92 00 8E 00 00 D8 0A |
91 00 13 08 20 0A |
92 00 14 FF FF F8 69 |
92 00 14 00 00 F9 D9 |
82 00 14 00 00 38 1A |
81 00 02 00 29 5C |