This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195: Question about REGN capacitor

Part Number: BQ24195

Hello, I have a customer who is designing the BQ24195 into their system, and they have used a 10uF capacitor from the REGN pin to GND. The datasheet specifically states to use a 4.7uF capacitor for this, but they would like to continue with a 10uF cap because it simplifies their BOM. Is this 4.7uF value absolutely critical here? Or would they be okay to use a 10uF capacitor? 

Also, if they use a 4.7uF.. would 20% tolerance be acceptable?

Thank you,

Daniel