This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61280D: failure event

Part Number: TPS61280D


Hi team,

When the failure event occur, the device have two performances, one is Vin=Vout and the other is Vout =0V.

Could you kindly explain under what situation will cause theses two different performance?

Thanks and best regards,

Jamie

  • Hi Jamie,

    There are many situations that would cause these two failure phenomenon. For example, EOS between SW and Vout pins cause high-side switch short, so Vin=Vout. EOS at SW to GND and SW to Vout cause both high & low side switches short, so Vout = 0V.

    Please share the detailed schematic, layout, operating specifications so that we can help analyze the root cause. Thanks.