Hi Ti Team,
I am Abhishek working as a Design engineer in Analog & digital R&D section.
I have one query related to Power Mosfet, I have to control the Output by putting a electronic switch.
Input - 24V@200Amp.(Battery)
Output- 24V@120Amp Continuous, 200Amp Peak current.
I am connecting the input with output by XT150 Connector, But there are some spark is coming while connection, Because load is ESC with BLDC motor.So it will draw approx 5-10 Amp current while connectingh the battery source.
I am planing to put a electronic switch operated with a micro controller having Power mosfet in parallel, which can handle the 200Amp current rating.
Kindly suggest some Power mosfet part no as per solution, Suggest some idea to implement this circuit.
Thanks
Abhishek Kumar
Design Engineer.