Hi,
In the data sheet Section 8.5, page 8, it is given that Vocd is programmable.
https://e2e.ti.com/support/power-management/f/196/t/857753 this post says that it cannot be programmed.
Can it be programmed by user or not?
if i need the device to support 8 A discharge current, as said by the post, ( VOCD1= 60mV if bq7791500 is chosen)
60mV/ 8 A = 7.5mohm.
So, i need to choose 7.5mOhm sense resistor to let the device support 8 A?
Why do we have VOCD1 and VOCD2? What is the purpose of having two VOCD values?
Thank-you
Warm regards
Harini Krishna