My ULN2803A connects a resistive load and an inductive load with differenent channel. The two loads are powered by the same 48V voltage source, which is provided by an adapter. The COM pin is also connected to the 48V power. I do not place any capacitance to the 48V voltage source. The upper limit of VCE of ULN2803A is 50V, which is only 2V larger than 48V power. Will it be too dangerous to do so considering the switches of the resistive load and the ripple and inaccuracy of the adapter? Should I add capacitance to the 48V voltage source?