Hello expert,
I would like to check if we have solution could support 3.6V~4.2V -> -5.3V/0.8A with inverting Buck-Boost topology. It would be better to have reference design for this application. Thanks a lot!
Best regards,
Ann Lien
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello expert,
I would like to check if we have solution could support 3.6V~4.2V -> -5.3V/0.8A with inverting Buck-Boost topology. It would be better to have reference design for this application. Thanks a lot!
Best regards,
Ann Lien
Hi Ann,
I couldn't find any buck-boost device matching the requirements, the most we can achieve for those voltages is around 200-300 mA.
There might be a suitable buck converter that can be configured as an inverting buck-boost, I will check with the buck team.:
http://www.ti.com/lit/an/snva856/snva856.pdf
Best regards,
Milos
Hello Ann,
I found only this reference design that can fit your case. Here there is the link for TIDA-01457 based on the module TPS82130.
Hello Alfonso,
It seems like we can use simple 3A converter solution to achieve it. May I use TPS62826 which is already used in their application to achieve 3.6V~4.2V -> -5.3V/0.8A application? Thanks a lot!!
Best regards,
Ann Lien
Hi Ann,
The TPS62826 cannot be used, its Vin_max is 5.5 V which is not high enough. When used in inverting buck-boost configuration, the Vin_max requirement is:
Vin_max = Vin + |Vout| = 4.2 + 5.3 = 9.5 V (for explanation check Figure 5 from the document I linked above)
You might use the TPS62130, check Section 9.3.3 from the datasheet, and this application note for calculations:
http://www.ti.com/lit/an/slva469c/slva469c.pdf
For your input/output voltages it should be able to provide at least 1 A, but double check with the buck team if there are any other concerns.
Best regards,
Milos
Hello Ann,
Thanks, Milos, for the explanation. Last time you look for a solution with a reference design, and I provided the link of TIDA-01457. On the first page, it is specified that the solution works at around 1A. Also, tps62130 can be suitable for your application, but is available only a ref design that doesn't match your rails (TIDA-01423).
For specific support on these devices, please open a new thread, including the part number since I am supporting buck converter below 7V.