We are using LM5071 part in 3rd mode (min ripple configuration) for the rating 6V,0.6A. We are using transformer primary winding as an inductor for the same. Below are some detials -
VIn= 24V
Vout= 6V, 0.6A
Fsw= 580Khz (RON=115K).
With the above configuration, the switcher is not working properly and giving 0.348V output. Please do let us know, why we are facing this issue, is there any resolution for this.
Please find attached datasheet of transformer.