Other Parts Discussed in Thread: TPS61088
Tool/software: WEBENCH® Design Tools
Hello TI,
We are working on our Own BMS design system which have BQ24773, BQ27542 and TPS61088.
We looking to avoid battery leakage when it is not in use .
When the system Operated in battery power state with load and battery is goes below to the minimum system voltage, therefor load is need to disconnect from BMS(Power source), but the BMS steel ON and it's drain the battery till reach at depleted, we want to shutdown the BMS when battery voltage goes below the Minimum system voltage.
There is any Disable option in BQ24773 to avoid Over discharging the battery pack ..?
There is any Identification parameter in BQ24773 register command set for Battery charging and discharging Done notification to host controller ..?
What is suitable option to implement above mention feature in our BMS ..?
In our System we don't have required number of ADC to read the BQ24773 parameter like IADP, IBAT and PMON, we are looking for the I2C based ADC IC please suggest us suitable part to our design, currently we are selected ADC128D818CIMTX
Thanks and regards,
Rahul Surawase