This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ77915: fault recovery problem

Part Number: BQ77915

Hi,

We are testing a 3s2p configuration with BQ7791500. 

We followed the EVM and connected resistor divider with a power supply as a replacement of the battery.

1) for over voltage the device was just working fine. 

2)While testing for OW fault, We removed one of the connection  and the device entered the fault state

When we tried recovering the fault state by reconnecting the removed connection the fault state was not recovered. 

The fault  recovered only when the power source is disconnected and connected again.

3) for under voltage test condition, it was not recovering from the fault condition even after meeting the recovery conditions. To recover the fault condition again the power supply had to be disconnected and reconnected again. 

 4) For UV fault recovery the suggested method for fault recovery is load removal. We have an application where we cannot disconnected the load ( remove the load). So, instead of removing the load will connecting charger restore the fault condition or removing load is compulsory for recovering the fault conditions?

5) There are few other fault conditions where load removal is required. Our application doesn't support disconnecting of load. So is disconnecting of load compulsory of load recovery or is there any method to recover the fault conditions without disconnecting / removal of load?  

6) How to know if the IC is burnt out? We burnt out 2 ic's already.  The third one DSGfet gate signal gives 0V and CHGfet gate signal  gives 2.53 V  no matter which state it is in. 

 the device doesn't come out of fault conditions for OW and UV fault conditions. 

Could you please help me in understanding  why the device is behaving this way?

Thank-you

Warm Regards

Harini Krishna

  • Hi Harini,

    The device should be able to recover from these faults without cycling power. Make sure all of the conditions for recovery are met (hysterisis and time) and it is possible to recover by connecting a charger (see the Design Example in the datasheet which targets this requirement).

    If you are damaging ICs, there is possibly something wrong with your schematic. Carefully check the datasheet to make sure you have everything connected correctly and that you are not violating Abs Max on any of the device pins.

    Regards,

    Matt