Other Parts Discussed in Thread: LMR33610
I intend to use the TPS61022 to boost the voltage from a super capacitor to 5.05V at the output.
In order to "bridge" the charge time of the super capacitor I will use the LMR33610 to provide the 5.05V output during the charge time of the super-cap.
Questions:
This "back-drive" of voltage across the TPS61022 during the 60s charge time how will this effect the IC?
What level of current will run back from the output pin into the TPS61022 when the input voltage (super capacitor) is 0V?