This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510-G3: BQ27510-g3 df.fs and bq.fs is fail to flash and stuck in rom mode

Part Number: BQ27510-G3

Hi

we  are using bq27510-g3 with AM43xx.

I try to flash configuration image (df.fs)  but it's not successfully flash and stuck  in ROM mode.

after debug we  found it's fail because of checksum fail at following part of image.

 

W: 16 00 02 00 00 00 EA FF 33 24 FA 33 B8 FA 33 3D FE 33 45 FE 33 FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F FF FF 3F 00 04 3F 58 CB 33 DB 00 08 00 00 00 00 00 00 FF AA 0E FB A7 0E FF A6 0E FF A1 0E FF A0 0E FE A3 0E 77 A2 0E D2 FF 3A FF A1 0E 66 A0 0E FF A3 0E
W: 16 64 1B 35
X: 2
C: 16 66 00 // fail on this 

It's geting 0x02 instant of 0x00

Also Try with i2c command line but same problem.

i2cset -f -y 0 0x0b 0x00 0x02 0x00 0x00 0x00 0xEA 0xFF 0x33 0x24 0xFA 0x33 0xB8 0xFA 0x33 0x3D 0xFE 0x33 0x45 0xFE 0x33 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0xFF 0xFF 0x3F 0x00 0x04 0x3F 0x58 0xCB 0x33 0xDB 0x00 0x08 0x00 0x00 0x00 0x00 0x00 0x00 0xFF 0xAA 0x0E 0xFB 0xA7 0x0E 0xFF 0xA6 0x0E 0xFF 0xA1 0x0E 0xFF 0xA0 0x0E 0xFE 0xA3 0x0E 0x77 0xA2 0x0E 0xD2 0xFF 0x3A 0xFF 0xA1 0x0E 0x66 0xA0 0x0E 0xFF 0xA3 0x0E i
i2cset -f -y 0 0x0b 0x64 0x1B 0x35 i // its geting i2c IO error  "i2cset: write failed: Remote I/O error"
sleep 1
i2cget -f -y 0 0x0b 0x66

Can you please review the same and help with your expert comments.