Hello,
We are using the BQ35100 in EOS mode with a lithum primary battery and we have 5 questions :
1) When we perform a "Gauge disable" and the a "Gauge enable" (using the pin 5), we loose the UNSEALED access. Then we have to UNSEAL each time we do a "Gauge enable", is it normal ?
(We don't remove the battery, so the BQ35100 still have power supply beetween the "Gauge disable" and the a "Gauge enable")
2) The chemestry programmation only affect the Ra table or it affect other parameters ?
3) We are planning to use the LSH 20 SAFT (13000 mAh) battery but it's not in the last chemestry tab (version 767). So we will not have the good Ra table.
Does it matter for EOS detection since it's based on relative evolution of the impedance ?
4) Concerning the SOH estimation, how can we have the best results without the good Ra table ? Or how can we determine by ourselve the good Ra table ?
5) What is the influance of the R Data Seconds parameter ? By default it's programmed to 15 seconds, can we shorten that to 1 second for exemple ?
Because for us it's a bit long to stay more than 15 seconds at constent consumption, waiting for "G_Done".
Thanks in advance for your reply