This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25066: current limit and circuit breaker difference

Part Number: LM25066


Hi,

customer have question about the difference between current limit and circuit breaker.

they need to set bus overcurrent production, once over current, turn off the MOS, if the current go to normal, turn on the MOS.

my understaning is the current limit is to limit current, can't off output, right?

I recommend customer use circuit breaker as OCP threshold, could you help double confrim and give your suggestion?

thank you

  • Hi Betty,

    Current limit is the value to which the Hotswap controller limits the current during startup by controlling the Gate of the FET.

    During steady state, if the load current value goes above the set current limit (but less than the circuit breaker threshold), the hotswap allows the current to pass for the timer duration and then turns OFF the FET.

    If the load current goes above Circuit breaker threshold, the FET's are turned OFF immediately. 

  • Hi Betty,

    Hope your queries are answered. Please let us know if you have more questions.