Greetings,
May i know if tps54360 external components such as capacitors, resistors have a specific requirement ?
For example, C1 , C2, can i just use any capacitor with the specified capacitance without
concerning the max voltage by the capacitance ? If i need to take into considerations, what would be the voltage required for all the components ?
For me, i just would like to have an input of 40 -60V with output of 5V and 3A. Just as the typical applications.