This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075: BQ24075

Part Number: BQ24075
Other Parts Discussed in Thread: TPS61022, , BQ24074, BQ24073, BQ24078, BQ24076

Hi,

        We are going to design a GPS tracker using 3.7V li-ion battery as well as 5V DC  charger input.

1)TPS61022 as Buck boost for VBAT(4V)  for GSM part. and that 4V convertered into 3.3V through a LDO for GNSS part.

2) Since BQ24075 VREG output =5.5V the TPS61022 cannot support  5.5V input.

3) We need SYSOFF  pin also.

    Kindly provide a solution to this.