This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61235P: Efficiency Problem?

Part Number: TPS61235P


Hi, 

My setup including TPS61235P, BQ27441 Fuel Gauge and 18650 3500 mAh Li-Ion Battery.

When my load is 5V 2A, the battery current is rising 3A . (Battery voltage= 3.6V) . I am getting battery current value from Fuel Gauge. 

These values are normal?

TPS61235 efficiency is %50 with these values, right? But it should be higher than %90 according to datasheet?