Is LM5023 able to operate at more than 100KHz under these conditions?
Input voltage : 100V
Output voltage : 20V
Output current : 3.25A
I know a bit of knowledge about designing the inductance value of the flyback transformer.
so I would like to know just whether or not LM5023 is able to work at that frequency.