Part Number: BQ25896
Other Parts Discussed in Thread: BQ21061, , BQ25606
Hi,
Could you recommend proper device?
The requirements are as below.
5V, 2A charging
5V, 100mA and 3.3V, 300mA output
Standalone
During the charging, output is enabled.
If output can't be enabled, output is automatically disabled when charging is enabled.
BQ21061 has LDO port but it is controlled by I2C.
For BQ25896, it seems to be realized with 3.3V LDO.
1. When USB is connected and VIN is 5V, is OTG output disabled automatically?
2. For 5V output, can PMID pin be used or VBUS?
3. Is there any other recommendation?
Thanks.