Hi guys,
As we saw the posts regarding learning cycle, the learning cycle has been completed successfully for now.
But I have doubt regarding managing self discharge or auto discharge of cells. In BQ34Z100-G1 is there any possible pin or block which helps me to estimate or re calibrate the cells. As we know "Self-discharge of NiMH batteries is estimated based on an internal timer and temperature sensor", is there any possible solutions with BQ34Z100-G1 and is there any related document which supports self discharge.
Our Battery pack Specifications
Series: BK220SCHU
Nominal Voltage:1.2 V
Rating Capacity: 2200 mAh
Cell Chemistry: NiMH
Charging: -deltaV per cell is 5-10mV (cell)
Rapid Charge temperature: 0-60 degree C
Discharge temperature: 0-75 degree C
ChemID: 6112 (TI suggested).
Battery pack configuration: 10S
Thanks in advance!!
Regards
Reddy