Hi
I'm using the TPS40210 as a boost converter. Actually, I'm working on an unmodified 40120EVM board atm.
I need to dynamically adjust the output slightly and my plan was to inject a +/- 700mV voltage to the FB pin (from an INA213 current monitor). The plan was to keep the feedback resistors in place, as the signal from the current monitor will be interrupted frequently.
However, the TPS40120 starts resetting when I connect the INA213 output. Is the above not a valid approach? It feels like I'm overlooking something basic here...