This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27750: Compatible with BQ24075?

Part Number: BQ27750

I am working on the battery charging system of a product we are developing.  We use the bq24075 to charge a single Li battery.  Inside the battery is a bq27750 battery gauge chip.  What can we expect the interaction of these two chips to be if you can answer, and is there a problem using them in this way?  Our problem is that we have seen situations where the battery is not charging.  We need input on conflicts that are possible which could cause a failure to function as desired.  We need to understand the characteristics of the interaction to avoid it if possible. Thank you