Hi,
I want to clarify below two points.
1) I want to know how to calculate the the power dissipation for gate series resistor.
I did as below.
Gate Voltage(V): 12V
Gate series resistor(R): 16.5R
Mosfet Total Gate charge (Qg): 331nC
Switching Frequency(F): 12kHz
Gate current:
V/R = 12/16.5 = 0.727 A
Gate voltage rise time:
Q=I*t
Gate voltage Rise Time (tr) =331nC/0.727 = 455nS
R16.5 (power dissipation) = V*I = 12*0.727 = 8.7W for 42uS for 50% duty cycle of 12kHz
Is this correct?
2) Can i consider the pulse power limitation for meeting the power requirement in above case. But its withstanding limit only for short period of time 8000Hrs mentioned in datasheet (refer below link, page 5 continuous pulse power)
http://www.vishay.com/docs/20043/crcwhpe3.pdf
Please advice how to go about with the Gate resistor selection.
Thanks & Regards,
Suresh.