UCC28070 - About VAO pin
Hi Team,
I have three questions for VAO pin.
---------
[Q1]
I understand that VAO pin is Voltage Amplifier Output.
And “VVAO represents the total output power of the PFC preregulator.”.
I understand that Voltage Amplifier don’t monitor the output current but monitor the output voltage.
However, behavior of VVAO is as follows.
-if output current increase, output voltage decrease and VVAO increase
-if output current decrease, output voltage increase and VVAO decrease
( VVAO : 1V at zero current and full output current is 4.2V.)
Therefore, VVAO can represent total output power.
Is my understanding correct?
---------
[Q2]
I understand that “the UCC28070 has been designed to improve its transient response by pulling up on the output of the voltage amplifier (VVAO) with
an additional 100 μA of current in the event the voltage on VSENSE drops below 93% of regulation (2.79 V).”
so, if VVAO is clamped at 5V and this status continues being maintained, output current is abnormal(over current).
Is my understanding correct?
---------
[Q3]
I understand that If VVAO is more than 4.2V (for example, VVAO is 4.5V), output current is abnormal(over current).
Is my understanding correct?
<datasheet page.27>
Although the maximum VVAO is clamped at 5 V, at full load VVAO may vary around an
approximate center point of 4.2 V to compensate for the effects of the quantized feedforward
voltage in the multiplier stage (see Linear Multiplier and Quantized Voltage Feed
Forward for details). Therefore, 4.2 V is the proper voltage to use to represent maximum
output power when performing voltage-loop gain calculations.
---------
Regards,
Hide