This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: GPIO Addressing

Part Number: BQ79606A-Q1

Just would like to clarify. 

1. Do we leverage GPIO high/low state to set device address? 

2. Which GPIO state is MSB for address? for example, if [GPIO1,GPIO2,GPIO3,GPIO4] state is [1,1,0,0], the address is 0xC or 0x3? 

3. Do we have internal pull-up or pull-down for GPIO? The question is what's the GPIO state when it's float? 

4. If we need to pull-up or pull-down for GPIO, what's the recommend pull-up or pull-down resistor value? 

  • Hi Beginner,

    Please read over sections 9.2.1.2.13.3 GPIO Addressing and 8.5.2 General Purpose IOs and SPI of the datasheet for several of your questions. Also read over the EC table for details on weak pullup/pulldown values spec. If something is unclear in these sections, please open a new thread.

    Regards,

    Taylor