This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381A-Q1: Do I have to communicate with the device to get the output rails I need?

Part Number: TPS65381A-Q1

Hello,

I'm looking into using this device to power a Hercules MCU and another device that needs 5V input.

Is it possible to configure this device in hardware to give 1.2V, 3.3V and 5V outputs? Or do I have to use SPI to configure the device to produce these outputs? I want to avoid having to communicate with the device.

Regards,

Leslie