This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

0% --> 100% soft-start

Other Parts Discussed in Thread: UCC2800

Hi, Ti EE

i'm developing a telecom power converter having soft-start function to limit current and it also could be like a switch. showed as below

0% --> 100% PWM behavior likes Current limit mode.

100% PWM behavior likes Switching (just bypass)

I try to design it by UC284X, but i can't meet 100% PWM.

 pleas recommend part-umber to help me design. remarked by blue.

the require spec :

1. 0% --> 100% PWM ,soft-star

2. have a external disable pin 

3. OCP function

4. without feedback is ok.

thank you