This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC2526: PWM IC for Blinking LED light application

Part Number: UC2526


Dear Sir,

I am looking for PWM IC.Which will generate frequency in the range from 0 to 15 Hz for Blinking LED light application.

With UC2526 achieved up to 30 Hz. I didn't get PWM signal 30 Hz with R = 150K and C= 20uF.

Kindly suggest suitable IC which suits for our blinking LED function.

Regards
Murthy