This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: About the resistance value used in EN and UVLO

Part Number: LM5116

Hi,

I previously asked in the following thread about the resistance values used for EN and UVLO in the LM5116 circuit.
In the circuit above, I will eventually use the following resistor values:
Can you give me your opinion if I am OK with this resistance value?

UVLO pull-up: 10kΩ
UVLO pulldown: 1.8kΩ
EN pull-up: 10kΩ
EN pull-down: 10kΩ

Best regards,

e2e.ti.com/.../886026

  • HI

    Pls notice that: the maximum EN transition time for proper operation is one switching period. For example, the enable rise time must be less than 4 μs for 250-kHz operation

    and base on your UVLO resistor value, LM5116 will shutdown when 12V drop down to around 8V.

    The resistor value is fine.  

    Thanks