I am designing a high current dc-dc stage for a charging dock. I have an external 19V brick psu. My dock will cater for qty 5 x 5V 2A charging receptacles. Am I best advised to use qty x1 dc dc converter giving 5V 10A output (based on TPS40195)? Or might I be better off having 5 individual point of load converters each rated for 5V 2 A.
Is it mainly a BoM cost decision? Or are there other technical considerations which would favour one approach over the other?