Dear Support,
My customer is looking for a 1.8V to 5V level translator, with a low quiescent current and just one power supply. The 1.8V signal is a simple information 0 or 1, with no specific data rate and doesn't need any specific output current (just used to bias another IC).
We get the idea to use the TPS22917, applying a 5V on Vin and the signal on the input "ON".
Do you confirm that the input thresholds allow this kind of use?
Do you see anything which is not recommended in that case?
Regards,