Other Parts Discussed in Thread: LM358
Dear Sir,
We are using UC2526 to control the Buck output voltage as per the attached schematic.
Pin no: 1 of UC2526 error amplifier is set to 5V as a fixed reference.
Pin no: 2 of UC2526 error amplifier is connected to 4N35 Collector (will vary based on feedback from 0 to 5V).
we are using Type II Compensator to stabilize to loop
External feed back input signal pass through LM358, BC547 and 4N35 to the Pin no: 2 of UC2526 error amplifier.
Output signal from 4N35 output will be square wave (not pure analog signal)
will this flow of schematic attached will adjust the duty cycle to regulate the output voltage ??.
Please verify the schematic and suggets the your Valued inputs to achive the regulated PWM.
Regards
Murthy